This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24392: The reason for CHG_DET not detect

Guru 19685 points

Part Number: BQ24392

When testing bq24392 for BC detection, sometimes CHG_DET not become high.

(USB cable is compliant BC standard)

Datasheet page 9: “8.1.1.4 Slow Plug-in Event” is described that D+/D- detect during 600ms is OK, but CHG_DET is not output.

I didn't find the other D+/D- condition on datasheet information.

Please let me know the idea for find reason or points of need confirmation.

Waveform for NG and OK are attached below;

・NG: DP/DM is connected after VBUS startup to 175ms, but CHG_DET is not become High

・OK: CHG_DET become High after VBUS startup to 135ms.

Best regards,

Satoshi