Part Number: TS3DV642-Q1
Hello,
is there any further information about the propagation delay of the device. Is there a maximum value?
Our idea is to use two of these devices to switch the input from two deserializer (A and B) with odd and even pixel lanes to a receiver (R)
This would mean that one IC will switch between even pixel lanes of A and B to R while the second IC will switch the odd pixel lanes same way.
Is it feasible or the propagation delay could cause malfunctions?
Thanks for your support,
Luca