Part Number: TLK100
Hi, I'm experiencing issues with this component during startup in cold conditions (-23 degrees Celsius).
We have used several hundreds of these in our pcb's for the past 5 years, but during a startup in cold environment we are now experiencing issues.
It seems that the oscillator starts up, but the controller itself does not - and it does not provide a 25MHz reference out either (to provide a clock reference for the next PHY circuit)
After a reboot, everything seems to work as it should and it takes a couple of attempts to replicate this issue, and somethimes it seems to help to allow the PCB to cool down before a new issue arises. Of the 20 boards in test, only one or two seems to have this issue....
Do anyone have any errata information on this IC regarding temperature?
/Best Regards
Eirik Larsen