Part Number: PCA9517
I have two questions about the PCA9517.
(1) Do you have any requirements regarding "the power off sequence"?
(2) Do you have any requirements regarding "the timing of power and EN"?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCA9517
I have two questions about the PCA9517.
(1) Do you have any requirements regarding "the power off sequence"?
(2) Do you have any requirements regarding "the timing of power and EN"?
Hello Kensuke,
(1) Do you have any requirements regarding "the power off sequence"?
PCA9517 has built in powered-off high impedance I2C pins. This means that when VCCB and/or VCCA = 0V, all inputs and I/Os are over-voltage tolerant up to 5.5V.
(2) Do you have any requirements regarding "the timing of power and EN"?
The EN pin is an active-high enable with an internal pullup to VCCB. Upon powering VCCB, automatically powers up EN to be set HIGH. It is highly recommended not to change the state of the EN when communicating otherwise the bus could hang up. Only change EN when the I2C bus is in an idle state.
There is no order of powering up required for the EN pin when powering VCCA or VCCB. VCCA or VCCB can be applied in any sequence at power up. An internal power-up circuit keeps the output drivers turned off until VCCB is above 2.5V and VCCA is above 0.8V.
Regards,
Tyler