Part Number: TLK6002
Hi,
I am configuring TLK6002 as per below settings and i am sending clock and data from ZCU106.
LINE RATE = 2457.60
PLL Multiplier = 20
Rate Select = Half
TXCLK_A = 122.88
Ref_Clk = 122.88
Q1: I am configuring rate select as half rate but after reading control register 1 rate select is showing as Full rate.
Q2: I am following 20-Bit Interface Mode, here AGS is not locking.
Q3 : Channel sync is not happening.
Thanks & Regards,
Mallikarjuna B.