Part Number: TPD6S300A
I have seen that I can use the C_SBUx lines to protect the Dx lines but in that case should I still connect the ESD protection and does the 4.5V (typ) overvoltage protection don't pose any problems ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPD6S300A
I have seen that I can use the C_SBUx lines to protect the Dx lines but in that case should I still connect the ESD protection and does the 4.5V (typ) overvoltage protection don't pose any problems ?
Hi Eric,
I'm not sure if I'm understanding your question properly, can you elaborate what do you mean by "still connect the ESD protection"? As you mentioned, the C_SBUx lines can be used to protect the Dx lines of the USB2. Phy to protect the USB2.0 pins instead.


In a CCx or SBUx short to VBUS, the TPD6S300A has 30-V tolerant overvoltage protection FETs integrated internally with fast turnoff time (70ns) and voltage clamps on system side to prevent any damage to the internal system of the CC/PD controller.

Thanks and Regards,
Raymond Lin
Thanks for your answer Raymond.
I am going to better detail my question.
My idea is to connect the USB 2.0 DP (or DM) signal with C_SBU1 (or C_SBU2) and D1 (or D2) for improving ESD protection from 6kV to 8kV.
Does the parasitic capacitor added by D1 (or D2) lower too much or not the bandwidth of the internal switch of C_SBU1 (or C_SBU2) ?
Hi Eric,
Thank you for the clarification, let me check internally to see if the parasitic capacitor has any effect on the internal switch. I'll get back to you latest end of week!
Thanks and Regards,
Raymond Lin
Hi Eric,
Apologies for the delay response, D1/D2 cap should not effect the internal switches for C_SBU1/2.
Thanks and Regards,
Raymond Lin