Part Number: TMDS181
Hi all. Curious if anyone has run into this similar issue failing Voff compliance test measurements on the data lines using the TMDS181 with the Keysight DSAV164A. For other video sources with no TMDS181, this test passes fine with readings ~0mV. The limit is -10mV <= value <= 10mV. However, when using the TMDS181 eval board and also on our own design, we are getting readings ~15mV on D0+. Voff Clock +, Clock -, and D0- pass but ~6-9mV. I tried power savings mode in I2C mode but that did not seem to have any impact. Maybe there are other tricks to bring this down closer to 0mV?