Part Number: TCAN1042H
Other Parts Discussed in Thread: ISO7741, ISO1044, ISO1042
Hi Expert,
My customer just want to ask the ISO7741 can connect with our CAN FD TCAN1042 or not ?
Or we have combo solution for this application ?
Eddie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eddie,
The Isolation team makes an isolated TCAN1042 and TCAN1044 called the ISO1042 and ISO1044. If you need the 70V bus fault protection then the ISO1042 comes with that bus fault protection.
Best,
Chris
Hi Expert,
I have another question if my customer want to use discreet solution like ISO7741 + TCAN1042 or TCAN1044. Is it make sense ?
Eddie
Eddie,
Your customer could do that if they like. Make sure that all the digital pins and voltage rails are separated correctly. Make sure you are not violating any of the specs of either device.
We are currently working on some collateral that goes over a set up just like this. But it will not be ready for a couple months.
Best,
Chris