Part Number: DS250DF230
Hi,
Our customer operates under the following conditions.
1. Is there any guarantee that it will work under these conditions?
・Data Rate Range = 2.4756Gbps
・Frequency = 25MHz
・Register Address = Setting
0x09 = 0x04,
0x18 = 0x10,
0x60, 0x61 = 0x26,
0x62, 0x63 = 0xB1,
0x64 = 0xFF
Also, the thread below says "By setting it to CDR Bypass Mode, 2.4756 Gbps may be operated."
2. Please tell me the register to check CDR Bypass Mode setting.
3. Please tell me the register to set CDR Bypass Mode.
Best Regards,
Nishie