Other Parts Discussed in Thread: DS90UB948-Q1, ALP, DS90UB947-Q1
Hello,
I'm having a problem getting a link with 1080p60 resolution between DS90UB949-Q1 and DS90UB948-Q1.
Whenever I set the refresh rate to 60Hz (TMDS Clock of about 142MHz) the link is lost to the deserializer.
The Link works fine with refresh rate of about 42Hz (TMDS Clock of 100MHz).
The Pattern generator in ALP also uses 100MHz Clock for 1080p60 mode which is really not 1080p60
According to the datasheets the link supports up to 170MHz in dual link mode, but it seems I can't get it to work.
I can see in ALP that link is active and in Dual FPD3 mode, but once HDMI clock go to the higher value, the Link to deserializer is lost.
it recovers when the refresh rate is reverted to the lower value.
I have another combination with DS90UB947-Q1 and DS90UB948-Q1 that just works fine with the 60Hz refresh rate.
I don't know what I'm doing wrong here, can you please support in that?
Best Regards
Moamen