Part Number: TUSB2E22
Other Parts Discussed in Thread: TS3USB31E, TUSB216
Is it possible to connect two TUSB2E22 devices back to back to make a USB2 repeater. Connection would look like this:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks, this is what I suspected but wanted to confirm. We are aware of the USB2 redrivers like the TUSB216. The challenge is that there is requirement to disable the USB interface and there are two USB ports this needs to be done. A redriver like the TUSB216 could do this if combined with a USB SPST switch like TS3USB31E, but would take four devices for two channels. The back to back TSUB2E22 would only take two devices.
Hi Mark,
I double-checked with the system engineer that the TUSB2E22 cannot be used this way.
Regards,
Nicholaus
Hi Nicholaus,
Thanks for checking. We'll use the TUSB216 redriver with a SPST switch.