Part Number: DP83848J
Hi,
For the DP8384J needs to check TX/RX the rise and fall time or setup and hold time only?
seems only "PMD output Pair" needs to checked(T2.8.1)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kyle,
Can you please give me a background and what is the goal of these checks?
What do you mean by TX/RX? Do you mean TX_CLK, TX_D[3:0] and RX_CLK, RX_D[3:0]?
--
Regards,
Gokul.
Hi Gokul
I want to check "AC Timing Requirements" of RX/TX & Ref CLK have rise/fall time require.
due to i find the PMD seems needs to check rise/fall time, but TX_CLK, TX_D[3:0] and RX_CLK, RX_D[3:0] no needs to check.
Hi Kyle,
At a system level, You have to make sure that data setup and hold times are met.
You can also measure PMD rise fall times/duty cycle, VOD, but I would say all these are optional.
--
Regards,
Gokul.