This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90C387: DS90C387VJDX/NOPB - 10 Channel LVDS/Clock Interfacing with TFT.

Part Number: DS90C387

Good Afternoon,

I am designing a Hdmi to LVDS bridge and am having issues understanding how the connections from DS90C387VJDX/NOPB LVDS outputs should be connected to my TFT (i have attached for reference).

I have 8 differential data outputs (A0 to A7) and 2 differential Clock outputs (which are identical so can be interchanged).

My TFT requires that i provide 4 differential channels to provide the Odd data (OLVx), and 4 differential channels to provide the Even data (ELVx).

Which of the outputs from DS90C387VJDX/NOPB differential channels provide the odd data (that i can connect to OLV0 to OLV3) and which do i conect to the even (ELV0 to ELV3).

I appreciate any clarity on the matter as pg18 and pg19 are not clear.

www.ti.com/.../ds90c387.pdf

How am i to deduce if the TFT should be driven in DC-Balanced or Non-DC-Balanced mode?

I have provided Voltages/Logic input into configuration pins on the IC for reference:

BAL = HIGH

DUAL = HIGH

PD = LOW

R_FDE = HIGH

R_FB = HIGH

PLLSEL = HIGH

PRE = NC

P10 TFT.pdf