Part Number: SN75DPHY440SS
Hi
Do we have CSI re-timer with polarity inversion?
I want to know if can I swap the port like below image? because the layout routing limit.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN75DPHY440SS
Hi
Do we have CSI re-timer with polarity inversion?
I want to know if can I swap the port like below image? because the layout routing limit.

Hi,
From the net name, is this a CSI-2 application?
For CSI-2
The DPHY440 supports 4 CSI-2 DPHY lanes plus a clock. Unlike DSI, CSI-2 does not have a back channel path. Because of this, there is no requirement on lane ordering. Because there is no lane ordering requirement, there are more combinations which can be implemented. All possible combinations are supported by the DPHY440. For all CSI-2 implementations, the polarity must be maintained between the CSI-2 Source and CSI-2 Sink. The DPHY440 does not support polarity inversion.
It also looks like you are not using DA2P/N and DB2P/N. In this case, I would recommend not using lane 0 but lane 2.
Thanks
David