Part Number: DP83848I
Dear Sirs,
My customer needs comments on DP83848I design. Their device is power monitor/meter of AC power.
1. when the network storm occurs, device LINK & ACT LEDs are turned off.
2. After device reboot, connect it to PC, the PHY still not work, LINK & ACT LEDs still off.
3. check the register: reg<0x0001> Bit 2 Link Status is "0"
Customer add a debug code to check if the link status is "0" and keep 10 mins, the device will be reboot.
This can fix the problem above but will have another issue:
1. Customer cannot know the link status is "0" caused by real network disconnect or due to PHY hang on.
2. with this debug code, the device will always reboot in the field test if the LAN cable did not attach.
May I have your help if there is any better solution or suggestion for customer?
Thanks.