Part Number: TCAN1145-Q1
Customer having below doubts regarding TCAN register writes over SPI. As per datasheet, TCAN needs 16 clock cycles for SPI write register; which will be 4 us if we consider SPI clk = 4 MHz, But if we keep the delay below 50 us , we are not able to write all the registers successfully.
What should be delay between two register write/read operations for TCAN 1145-Q1? (in case of single register write/read operation and also in case of read burst and write burst)