Part Number: PCA9306
Other Parts Discussed in Thread: THS4561, , LSF0102, LSF0101
I am currently looking for a solution to limit the output voltage of a differential opamp (like the THS4561) supplied with 3,3 or 5V when feeding its output to a high speed ADC that accepts a maximum voltage of 1.8V only. After evaluating some topologies with transistors, I noticed, that the PCA9306 features exactly the same topology that I inteded to use. Since I don't assume that any switching circuitry is inside that may cause interference and usually an integrated solution is more convenient that the discrete solution, my quesion is: Although not intended for this use case, is it possible to use the PCA9306 for analog signal limiting when interfacing an ADC driver to an ADC?
Best regards and thanks in advance,
Robin