hi,
i use the TLK1501 to do a fiber optical transmission . The front system is an ADC, the output of the ADC enters into a FIFO . THE output of the FIFO enters to TXDATA[0-15] of the TLK1501 . but the problem is that , the rate of the ADC is only 5 MHZ, and the rate of the TLK1501 is 30-75MHZ , so i use the TLK1501 rate 50 MHZ, i receive the data 5 times . So i want to know how to resolve the problem ? thank you very much!