Hi team,
- Could you kindly tell me how to configure CSI-2 timing at 1.2Gbps?
- Could you kindly tell me what is the max CSI-2 bandwidth per RX port of 662 and 964? 935 is 2.528, 954 is 3.328.
Thanks!
BR
Jiawei
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Thanks!
BR
Jiawei
Hello Jiawei,
1) What timing do you mean? We do not configure or recommend changing the CSI-2 timing.
2) The 662 has the same CSI-2 bandwidth of the 935, which is 2.528Gbps/ Rx port.
Hi Hamzeh.
Thanks for your reply.
1. 960 will auto set csi timing at 800 and 1.6gbps. But won't auto set at other csi rate. Datasheet only give 400Mbps configuration, how about 1.2G?
2. How about 964?
BR
Jiawei
1) Same thing for 1.2Gbps. You do not need to change anything! Only if using 400Mbps you should write the sequence in the datasheet.
2) In this case 1330Mbps/ Rx port. See section "6 Data Rate Calculations" on this Appnote.
Hi Hamzeh,
Thanks! Could you kindly help me check my summary excel, appreciate!
|
Deserializer Hub |
MAX CSI-2 Lane Speed |
CSI-2 Port |
MAX Output CSI-2 Bandwidth |
MAX CSI-2 Bandwidth Per RX Port |
|
DS90Ux936-Q1 |
1.664Gbps |
1*4 Lane |
6.656Gbps |
2.528Gbps |
|
2*2 Lane |
||||
|
DS90Ux954-Q1 |
1.664Gbps |
1*4 Lane |
6.656Gbps |
3.328Gbps |
|
2*2 Lane |
||||
|
DS90Ux964-Q1 |
1.6Gbps |
2*4 Lane |
12.8Gbps |
1.330Gbps |
|
DS90Ux962-Q1 |
1.664Gbps |
2*4 Lane |
13.312Gbps |
2.528Gbps |
|
DS90Ux662-Q1 |
1.664Gbps |
1*4 Lane |
13.312Gbps |
2.528Gbps |
|
DS90Ux960-Q1 |
1.664Gbps |
2*4 Lane |
13.312Gbps |
3.328Gbps |
BR
Jiawei
Hello Jiawei,
The 962 does not have 2x CSI-2 output ports. Just 1 port x4 lanes.
The 662 and 962 max output CSI-2 bandwidth is 6.656Gbps.
All ADAS devices are UB. There is no UH.
NOTE: the max CSI-2 output bandwidth does not mean that you can output exactly the same data rates. Because there will be some CSI-2 blanking, depending on the used Forwarding mode. Please refer, for example, to 960 d/s, section "7.4.20 CSI-2 Output Bandwidth".