This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUXHS4212: x16 PCIe Link through x8 Demuxed and x8 Non-Demuxed Lanes

Part Number: TMUXHS4212
Other Parts Discussed in Thread: TMUXHS4412

Hi everyone,

Is it possible to establish an x16 PCIe Gen3 link using this IC in a configuration where 8 of the 16 lanes are outputted from multiple instances of this IC and the other 8 lanes are directly routed to the CPU (Root Complex), without passing through the demuxing logic?

Below image shows a hand sketch of the intended connection:

Or is x8x8 bifurcation needed, since 8 lanes will pass through the demuxing paths and 8 lanes will not be routed through the IC?

Thanks,