Part Number: DP83849I
DP83849IVSのICについてご質問があります。
現在、DP83849IVSとルネサス系CPU(RX71M)を使用してLAN通信を2ch分、実現しようと考えています。
そこでMII通信のMDIOとMDCについてルネサス系CPU(RX71M)は2ch分ありますが
DP83849IVSには1ch分(共通)しかありません。
LAN通信を2ch分、実現しようとした場合どのような接続になるのでしょうか。
ご教授お願いいたします。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83849I
DP83849IVSのICについてご質問があります。
現在、DP83849IVSとルネサス系CPU(RX71M)を使用してLAN通信を2ch分、実現しようと考えています。
そこでMII通信のMDIOとMDCについてルネサス系CPU(RX71M)は2ch分ありますが
DP83849IVSには1ch分(共通)しかありません。
LAN通信を2ch分、実現しようとした場合どのような接続になるのでしょうか。
ご教授お願いいたします。
Hello,
Using a single channel of MDC/MDIO should allow for multiple PHYs to be programmed, as the channel is a multi-port bus system.
PHYs with different addresses can be connected and controlled by a single bus.
We are not aware of this CPU, please check with Reneas for more information on RX71M functionality and configuration.
Thank you,
Evan