Part Number: DS125BR401A
Production test without high speed signaling.
Is it possible to test the PCB where the 125br401A is used without using high speed signals??
For production test of the PCB where the 401A is placed, we don't have access to high speed signal, only lower ~200MHz signal, is possible to make a simpler function test?
It is a mezzanine board, that has two connectors front/back, and the 401A in between, the suggestion is to insert signal in one connector and loop it on the other connector back to the insertion connector, and validate the signal. Is that possible? Only for detecting the mounting of the connectors and 401A circuit.