This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA6418E: questions about pin terminations

Part Number: TCA6418E


Hello,

Q1:
When RESET_ pin is not used, how much ohms resister does TI recommend to pull up the RESER_ pin to Vcc?

Q2:
When INT_ pin is not used, can this pin be left floating (unconnected anywhere)?

Q3:
How unused GPIO pins are terminated?


Best regards,

K.Hirano

  • 1. For high-impedance CMOS input, this does not matter. You can use 0 Ω.

    2. Unused outputs can be left open.

    3. Unused outputs can be left open. Unused inputs should have a pull-up or -down resistor; you can use the internal pull-down, which is enabled by default.