Part Number: THVD8000
Hi ,
I am planning to use THVD800 for my new power over RS485 design, I need help with following things
1. Need a Pspice for TI model for THVD8000 part.
2. Is there a Maximum DC voltage current rating for A & B lines using this application.
3. How to calculate the Inductor value when there is a possibility to connect multiple devices on the bus (for example design the product to have 3 slaves connected to one master and circuit works fine with 1,2or 3 devices connected while still rated for say 80 mA load per device), do we have an application note around this.
4. How to do wiring between master and slaves (star/bus).
5. Can you assign any FAE for my case so that I can get the circuit reviewed
I have already done proof of concept with a point to point Master-slave config at data baud rate of 9600 and carrier frq of 115200 which works well for 24V DC supplying 80mA over a 100ft cable.