Part Number: P82B715
Other Parts Discussed in Thread: TCA9517, TCA9517A, ISO1540, PCA9306, LSF0102
Hi Team,
We plan to build a system as showing in the picture, could you help review does this work or there is any problem, thank you very much.
PCBA board a is host using 5V for I2C, has P82B715 buffer.
board b is slave I2C is 3.3V, has TCA9517 for voltage level translate and another buffer P82B715, and ISO1540DR for isolation, ISO1540DR VCC2/GND2 are from board a, VCC1/GND1 from board b itself.
board c, d, e, are same design with board b, but different I2C address.
board a will connect to board b/c/d/e at the same time using only one interface.
Pull up resistors are pending calculation. I2C speed is100Khz.