Part Number: DS320PR810
Hi
We have some queries for the Bias register(offset=0x06) in the DS320PR810 Equalizer:

1. For which circuitry inside the equalizer, this bias current is used for?
2. It is mentioned that "001" should be set to bit 5-3 for best performance. But if we don't write this value and keep it at default "100", what effect will it have on the device performance?
An early response will be highly appreciated.
Thanks,
Lalit