Part Number: AM26LV32
Hi Team,
The maximum output current,IO described is ".「±25mA(MAX)」" in AM26LV32 data sheet.
Is this a rated current per 1ch or a rated current total 4ch?
I think that "IOH" and "IOL" of "modified operating conditions" are "± 5 mA (max)",
but there is no problem even if 4CH is 10 to 15 mA.
Thank you.
Regards,
Frank