Part Number: DS250DF230
Hi,
Does the DS250DF230 support the following Ethernet transmission speeds?
・1000BASE-T (1000Mbps)
・2.5GBASE-T (2.5Gbps)
・5GBASE-T (5Gbps)
・10GBASE-LX (10Gbps)
・10GBASE-T (10Gbps)
Best Regards,
Nishie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS250DF230
Hi,
Does the DS250DF230 support the following Ethernet transmission speeds?
・1000BASE-T (1000Mbps)
・2.5GBASE-T (2.5Gbps)
・5GBASE-T (5Gbps)
・10GBASE-LX (10Gbps)
・10GBASE-T (10Gbps)
Best Regards,
Nishie
Hi Nishie-san,
Although the DS250DF230 can support 1 Gbps, 2.5 Gbps, 5 Gbps, and 10 Gbps, it is not suitable for base-T signaling. The DS250DF230 is designed for NRZ signaling, while Base-T typically implements more than two signaling levels. Because of this, it would not support the majority of the applications you mentioned above.
Regarding 10GBASE-LX, I could only find references to 10GBASE-LX4 in the IEEE802.3 specification. I'm not too familiar with 10GBASE-LX4. It looks like this is an optical specification that implements 4 lanes of data in order to achieve a 10 Gbps link. Can you clarify the electrical specifications that would be pertinent to this? Would there be 4 lanes of data at 3.125 Gbps, or just a single lane at 10.3125 Gbps? Would this be NRZ signaling?
Thanks,
Drew
Hi Drew-san,
Thank you for your support.
I get that the DS250DF230 is not suitable for Base-T signaling.
If possible, could you tell me which device supports 1 Gbps to 10 Gbps (Base-T)?
I will ask our customer about the 10 GBASE-LX lane configuration.
Best Regards,
Nishie
Hi Nishie-san,
Unfortunately, we do not have redrivers or retimers in our product line that are suitable for Base-T signaling.
Thanks,
Drew