Part Number: DS92LV18
Other Parts Discussed in Thread: DS92LV16,
Hi team,
I have a question using DS92LV18 (or DS92LV16) at cascase connection.
The product investigating is one master unit with multiple slave units. the distance between units are 10m~20m.
Master -> Slave1 -> Slave2 -> Slave3 -> Slave4 ------.
The DS92LV18 on the Slave units receives and transmits the recived 18-bit parallel deta to the next slave unit.
The whole system, one master and multiple slave units can afford max 1us signal delay and jitter.
Q1: Can one DS92LV18 receive and transmit same time?
Q2: For synchronization of all units, thinking pull SYNC to high for all units for a periods of time, but the period cannot be the same between units.
can it be workable?
Also appliciate if you provide any advises and concerns.
Regards,
Shiraki