Part Number: TRS3243
Hi Sir,
could help check this schematic is ok? if there any suggestion and learn form you.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TRS3243
Hi Sir,
could help check this schematic is ok? if there any suggestion and learn form you.

Tommy,
See Clemens's comment above. Also, based on your connection of FORCEON, it looks like you aren't using automatic power down since this pin is held high. This is fine assuming this is your intention.
Best,
Danny
Hi Danny,
thanks for you help and reply,
In addition, we have problems before, and the glitch that sometimes occurs before the system is ready will cause the COM PORT device to be abnormal.
So we will pull the shutdown pin of the transceiver, we pull PIN 22 now, is it ok?
Tommy,
Ok, understood. Using just pin 22 is okay, I just wanted to make sure this was intentional, and it sounds like it is.
Best,
Danny