This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB3210 sample source code kb3210.i2c and kb3210.bin



In the Keyboard firmware source code downloaded from TI there are two files  kb3210.i2c and kb3210.bin under \Release\Exe.

What is the file kb3210.i2c? If I used the Apploader drivers to load kb3210.bin to the tusb3210kbd rev3 it would work .

Was kb3210.i2c converted to kb3210.bin using Header.exe. If so how was that achieved?

 

  • Dang,

    I assume you have forgotten completely about this by now and I apologize.  this one got buried at the back of the forum and I just now realized we had not responded.

    Yes, the kb3210.bin is created using the header generator. This file includes the kb3210.i2c and the necessary headers.