Hi team,
I'm developing a PCB with the DP83822IRHBT.
I have a question about the characteristic impedance of RMII.
Section 9.2.2.2.2 states that the characteristic impedance of the pattern should be 50Ω.
The following signals are defined as RMII signals in Table 8-2.
TX_D[1:0]
RX_D[1:0]
TX_EN
CRS_DV
Is it okay to understand that there is no need to manage the characteristic impedance of the following signals?
MDC
MDIO
XI
RX_CLK
Best Regards,