Part Number: TUSB7320
There are cases where the USB 2.0 connection does not work when the power is turned on after the power has not been turned on (for about 1 hour or more).
2 out of 1000 units have this case.
・There is no data output of PCI Express of TUSB7320, and it does not link up.
・The connection sequence to the USB device does not start.
・The USB 3.0 port is unused.
I have confirmed that the power, clock, and reset signals are output according to the sequence described in the datasheet.
Any ideas why the USB connection doesn't work?
Also, if there is a sequence that should be confirmed other than the sequence described in the datasheet, please let us know.