Part Number: DS90UH948-Q1
When it is necessary to use vias in the FPD-Link trace, which impedance specification should be used for the vias: 100 Ω ±10% or ±20%?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UH948-Q1
When it is necessary to use vias in the FPD-Link trace, which impedance specification should be used for the vias: 100 Ω ±10% or ±20%?
Of course, the tight Impedance control is better!
I understood that the tight impedance control is better.
Per the "FPD-Channel-Requirements-DS90UH94xA_Rev0p5, impedance control requirements for PCB trace is 100ohm +/- 10% and the one for landing pad and component is 100ohm +/- 20%. Which number is applied for the vias, 10% or 20%?
Additionally, In case of eDP or other high speed signal traces, if I needs to use vias in traces, is the impedance cotrol requirements applied for the vias same as traces?
Thanks
Hello,
Vias are part of the PCB Trace, hence 10%.
Additionally, In case of eDP or other high speed signal traces, if I needs to use vias in traces, is the impedance cotrol requirements applied for the vias same as traces?
Yes, your PCB traces including vias should be impedance controlled!