Part Number: SN65DSI86-Q1
Other Parts Discussed in Thread: SN65DSI86, TDP142
Is there a EVM of the TQFP based SN65DSI86 device, can you please share the PCB files for the corresponding EVM? Thank You.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65DSI86-Q1
Other Parts Discussed in Thread: SN65DSI86, TDP142
Is there a EVM of the TQFP based SN65DSI86 device, can you please share the PCB files for the corresponding EVM? Thank You.
Sorry, we don't have TQFP EVM for this device.
Regards
Brian
Thank you Brian. for the quick reply. Currently, I am using the DSI Input --> SN65DSI86 (TQFP) --> TDP142 --> DP Connector. I have one question regarding the output HPD signal from the DP Connector to the input of the DSI86. Is it mandatory for the level translator, even though the VESA standard says the HPD signal is till 3.3V level? Can I understand that the HPD max signal level is 3.3V? Can you please tell me. Thank You.
You mean the max spec for HPD pin of DSI86 ? it didn't mentioned in datasheet. It can be 3.v or higher,but I don't think you need level shifter.
Regards
brian