What is the steady state current for this device TCAN1044AVDDFRQ1? I know the device operates at Vcc= 5V and if Vio is 3.3V. What is the maximum current this device can consume?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the steady state current for this device TCAN1044AVDDFRQ1? I know the device operates at Vcc= 5V and if Vio is 3.3V. What is the maximum current this device can consume?
Shashank,
The power consumption information is given in the Supply Characteristics section of the TCAN1044AV-Q1 data sheet. The highest current consumption case for this device would be during a bus fault (which is notably an abnormal condition) while attempting to drive a dominant signal, given as a maximum of 130 mA. See ICC > Supply current, Normal mode > Dominant with bus fault.
Best,
Danny