This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA8418: application issues.

Expert 2300 points

Part Number: TCA8418

Hi,

The current problem is that the key is not interrupted.

GPIO pins that are not used according to datasheet requirements need external pull-up resistor, but due to hardware error,

There is no pull-up resistor. Can I use a built-in pull-up resistor? How to set it?

thanks!

  • Pull-ups can be enabled in the registers 0x2C…0x2E; they are enabled by default.

    Please show how you have configured the device.

  • Hi Reed,

    Please check over Clemens' suggestions.

    This register information is found on page 34. of the datasheet.

    Regards,

    Tyler

  • Clemens,  Thanks! 

    /*
     * Driver for TCA8418 I2C keyboard
     *
     * Copyright (C) 2011 Fuel7, Inc.  All rights reserved.
     *
     * Author: Kyle Manna <kyle.manna@fuel7.com>
     *
     * This program is free software; you can redistribute it and/or
     * modify it under the terms of the GNU General Public
     * License v2 as published by the Free Software Foundation.
     *
     * This program is distributed in the hope that it will be useful,
     * but WITHOUT ANY WARRANTY; without even the implied warranty of
     * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU
     * General Public License for more details.
     *
     * You should have received a copy of the GNU General Public
     * License along with this program; if not, write to the
     * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
     * Boston, MA 021110-1307, USA.
     *
     * If you can't comply with GPLv2, alternative licensing terms may be
     * arranged. Please contact Fuel7, Inc. (http://fuel7.com/) for proprietary
     * alternative licensing inquiries.
     */
    
    #include <linux/types.h>
    #include <linux/module.h>
    #include <linux/init.h>
    #include <linux/delay.h>
    #include <linux/slab.h>
    #include <linux/interrupt.h>
    #include <linux/workqueue.h>
    #include <linux/gpio.h>
    #include <linux/i2c.h>
    #include <linux/input.h>
    #include <linux/input/tca8418_keypad.h>
    #include <linux/of.h>
    #include <linux/gpio.h>
    #include <linux/sunxi-gpio.h>
    #include <linux/of_gpio.h>
    
    /* TCA8418 hardware limits */
    #define TCA8418_MAX_ROWS	8
    #define TCA8418_MAX_COLS	10
    
    /* TCA8418 register offsets */
    #define REG_CFG			0x01
    #define REG_INT_STAT		0x02
    #define REG_KEY_LCK_EC		0x03
    #define REG_KEY_EVENT_A		0x04
    #define REG_KEY_EVENT_B		0x05
    #define REG_KEY_EVENT_C		0x06
    #define REG_KEY_EVENT_D		0x07
    #define REG_KEY_EVENT_E		0x08
    #define REG_KEY_EVENT_F		0x09
    #define REG_KEY_EVENT_G		0x0A
    #define REG_KEY_EVENT_H		0x0B
    #define REG_KEY_EVENT_I		0x0C
    #define REG_KEY_EVENT_J		0x0D
    #define REG_KP_LCK_TIMER	0x0E
    #define REG_UNLOCK1		0x0F
    #define REG_UNLOCK2		0x10
    #define REG_GPIO_INT_STAT1	0x11
    #define REG_GPIO_INT_STAT2	0x12
    #define REG_GPIO_INT_STAT3	0x13
    #define REG_GPIO_DAT_STAT1	0x14
    #define REG_GPIO_DAT_STAT2	0x15
    #define REG_GPIO_DAT_STAT3	0x16
    #define REG_GPIO_DAT_OUT1	0x17
    #define REG_GPIO_DAT_OUT2	0x18
    #define REG_GPIO_DAT_OUT3	0x19
    #define REG_GPIO_INT_EN1	0x1A
    #define REG_GPIO_INT_EN2	0x1B
    #define REG_GPIO_INT_EN3	0x1C
    #define REG_KP_GPIO1		0x1D
    #define REG_KP_GPIO2		0x1E
    #define REG_KP_GPIO3		0x1F
    #define REG_GPI_EM1		0x20
    #define REG_GPI_EM2		0x21
    #define REG_GPI_EM3		0x22
    #define REG_GPIO_DIR1		0x23
    #define REG_GPIO_DIR2		0x24
    #define REG_GPIO_DIR3		0x25
    #define REG_GPIO_INT_LVL1	0x26
    #define REG_GPIO_INT_LVL2	0x27
    #define REG_GPIO_INT_LVL3	0x28
    #define REG_DEBOUNCE_DIS1	0x29
    #define REG_DEBOUNCE_DIS2	0x2A
    #define REG_DEBOUNCE_DIS3	0x2B
    #define REG_GPIO_PULL1		0x2C
    #define REG_GPIO_PULL2		0x2D
    #define REG_GPIO_PULL3		0x2E
    
    /* TCA8418 bit definitions */
    #define CFG_AI			BIT(7)
    #define CFG_GPI_E_CFG		BIT(6)
    #define CFG_OVR_FLOW_M		BIT(5)
    #define CFG_INT_CFG		BIT(4)
    #define CFG_OVR_FLOW_IEN	BIT(3)
    #define CFG_K_LCK_IEN		BIT(2)
    #define CFG_GPI_IEN		BIT(1)
    #define CFG_KE_IEN		BIT(0)
    
    #define INT_STAT_CAD_INT	BIT(4)
    #define INT_STAT_OVR_FLOW_INT	BIT(3)
    #define INT_STAT_K_LCK_INT	BIT(2)
    #define INT_STAT_GPI_INT	BIT(1)
    #define INT_STAT_K_INT		BIT(0)
    
    /* TCA8418 register masks */
    #define KEY_LCK_EC_KEC		0x7
    #define KEY_EVENT_CODE		0x7f
    #define KEY_EVENT_VALUE		0x80
    
    struct tca8418_keypad {
    	struct i2c_client *client;
    	struct input_dev *input;
    
    	unsigned int row_shift;
    };
    
    /*
     * Write a byte to the TCA8418
     */
    static int tca8418_write_byte(struct tca8418_keypad *keypad_data,
    			      int reg, u8 val)
    {
    	int error;
    
    	error = i2c_smbus_write_byte_data(keypad_data->client, reg, val);
    	if (error < 0) {
    		dev_err(&keypad_data->client->dev,
    			"%s failed, reg: %d, val: %d, error: %d\n",
    			__func__, reg, val, error);
    		return error;
    	}
    
    	return 0;
    }
    
    /*
     * Read a byte from the TCA8418
     */
    static int tca8418_read_byte(struct tca8418_keypad *keypad_data,
    			     int reg, u8 *val)
    {
    	int error;
    
    	error = i2c_smbus_read_byte_data(keypad_data->client, reg);
    	if (error < 0) {
    		dev_err(&keypad_data->client->dev,
    				"%s failed, reg: %d, error: %d\n",
    				__func__, reg, error);
    		return error;
    	}
    
    	*val = (u8)error;
    
    	return 0;
    }
    
    static void tca8418_read_keypad(struct tca8418_keypad *keypad_data)
    {
    	struct input_dev *input = keypad_data->input;
    	unsigned short *keymap = input->keycode;
    	int error, col, row;
    	u8 reg, state, code;
    
    	do {
    		error = tca8418_read_byte(keypad_data, REG_KEY_EVENT_A, &reg);
    		if (error < 0) {
    			dev_err(&keypad_data->client->dev,
    				"unable to read REG_KEY_EVENT_A\n");
    			break;
    		}
    
    		/* Assume that key code 0 signifies empty FIFO */
    		if (reg <= 0)
    			break;
    
    		state = reg & KEY_EVENT_VALUE;
    		code  = reg & KEY_EVENT_CODE;
    
    		row = code / TCA8418_MAX_COLS;
    		col = code % TCA8418_MAX_COLS;
    
    		row = (col) ? row : row - 1;
    		col = (col) ? col - 1 : TCA8418_MAX_COLS - 1;
    
    		code = MATRIX_SCAN_CODE(row, col, keypad_data->row_shift);
    		input_event(input, EV_MSC, MSC_SCAN, code);
    		input_report_key(input, keymap[code], state);
    
    	} while (1);
    
    	input_sync(input);
    }
    
    /*
     * Threaded IRQ handler and this can (and will) sleep.
     */
    static irqreturn_t tca8418_irq_handler(int irq, void *dev_id)
    {
    	struct tca8418_keypad *keypad_data = dev_id;
    	u8 reg;
    	int error;
    
    	printk ("---Feibob: tca8418-irq-handle.\n");
    	error = tca8418_read_byte(keypad_data, REG_INT_STAT, &reg);
    	if (error) {
    		dev_err(&keypad_data->client->dev,
    			"unable to read REG_INT_STAT\n");
    		return IRQ_NONE;
    	}
    
    	if (!reg)
    		return IRQ_NONE;
    
    	if (reg & INT_STAT_OVR_FLOW_INT)
    		dev_warn(&keypad_data->client->dev, "overflow occurred\n");
    
    	if (reg & INT_STAT_K_INT)
    		tca8418_read_keypad(keypad_data);
    
    	/* Clear all interrupts, even IRQs we didn't check (GPI, CAD, LCK) */
    	reg = 0xff;
    	error = tca8418_write_byte(keypad_data, REG_INT_STAT, reg);
    	if (error)
    		dev_err(&keypad_data->client->dev,
    			"unable to clear REG_INT_STAT\n");
    
    	return IRQ_HANDLED;
    }
    
    /*
     * Configure the TCA8418 for keypad operation
     */
    static int tca8418_configure(struct tca8418_keypad *keypad_data,
    			     u32 rows, u32 cols)
    {
    	int reg, error;
    
    	/* Write config register, if this fails assume device not present */
    	error = tca8418_write_byte(keypad_data, REG_CFG,
    				CFG_INT_CFG | CFG_OVR_FLOW_IEN | CFG_KE_IEN);
    	if (error < 0)
    		return -ENODEV;
    
    
    	/* Assemble a mask for row and column registers */
    	reg  =  ~(~0 << rows);
    	reg += (~(~0 << cols)) << 8;
    
    	/* Set registers to keypad mode */
    	error |= tca8418_write_byte(keypad_data, REG_KP_GPIO1, reg);
    	error |= tca8418_write_byte(keypad_data, REG_KP_GPIO2, reg >> 8);
    	error |= tca8418_write_byte(keypad_data, REG_KP_GPIO3, reg >> 16);
    
    	/* Enable column debouncing */
    	error |= tca8418_write_byte(keypad_data, REG_DEBOUNCE_DIS1, reg);
    	error |= tca8418_write_byte(keypad_data, REG_DEBOUNCE_DIS2, reg >> 8);
    	error |= tca8418_write_byte(keypad_data, REG_DEBOUNCE_DIS3, reg >> 16);
    	printk ("---Feibob: configure TCA8418......\n");
    
    	return error;
    }
    
    static int tca8418_keypad_probe(struct i2c_client *client,
    					  const struct i2c_device_id *id)
    {
    	struct device *dev = &client->dev;
    	const struct tca8418_keypad_platform_data *pdata =
    						dev_get_platdata(dev);
    	struct tca8418_keypad *keypad_data;
    	struct input_dev *input;
    	const struct matrix_keymap_data *keymap_data = NULL;
    	struct gpio_config config;
    	struct device_node *np = dev->of_node;
    	u32 rows = 0, cols = 0;
    	bool rep = false;
    	bool irq_is_gpio = false;
    	int irq_pin, irq;
    	int error, row_shift, max_keys;
    
    	/* Copy the platform data */
    	if (pdata) {
    		if (!pdata->keymap_data) {
    			dev_err(dev, "no keymap data defined\n");
    			return -EINVAL;
    		}
    		keymap_data = pdata->keymap_data;
    		rows = pdata->rows;
    		cols = pdata->cols;
    		rep  = pdata->rep;
    		irq_is_gpio = pdata->irq_is_gpio;
    		printk ("---Feibob: irq_is_gpio = %d\n", irq_is_gpio);
    	} else {
    		int err;
    
    		err = matrix_keypad_parse_of_params(dev, &rows, &cols);
    		if (err)
    			return err;
    		rep = of_property_read_bool(np, "keypad,autorepeat");
    		printk ("---Feibob: ---------Feibob --------\n");
    	}
    
    	if (!rows || rows > TCA8418_MAX_ROWS) {
    		dev_err(dev, "invalid rows\n");
    		return -EINVAL;
    	}
    
    	if (!cols || cols > TCA8418_MAX_COLS) {
    		dev_err(dev, "invalid columns\n");
    		return -EINVAL;
    	}
    
    	/* Check i2c driver capabilities */
    	if (!i2c_check_functionality(client->adapter, I2C_FUNC_SMBUS_BYTE)) {
    		dev_err(dev, "%s adapter not supported\n",
    			dev_driver_string(&client->adapter->dev));
    		return -ENODEV;
    	}
    
    	row_shift = get_count_order(cols);
    	max_keys = rows << row_shift;
    
    	/* Allocate memory for keypad_data and input device */
    	keypad_data = devm_kzalloc(dev, sizeof(*keypad_data), GFP_KERNEL);
    	if (!keypad_data)
    		return -ENOMEM;
    
    	keypad_data->client = client;
    	keypad_data->row_shift = row_shift;
    
    	/* Initialize the chip or fail if chip isn't present */
    
    	error = tca8418_configure(keypad_data, rows, cols);
    	if (error < 0)
    		return error;
    
    	/* Configure input device */
    	input = devm_input_allocate_device(dev);
    	if (!input)
    		return -ENOMEM;
    
    	keypad_data->input = input;
    
    	input->name = client->name;
    	input->id.bustype = BUS_I2C;
    	input->id.vendor  = 0x0001;
    	input->id.product = 0x001;
    	input->id.version = 0x0001;
    
    	error = matrix_keypad_build_keymap(keymap_data, NULL, rows, cols,
    					   NULL, input);
    	if (error) {
    		dev_err(dev, "Failed to build keymap\n");
    		return error;
    	}
    
    	if (rep)
    		__set_bit(EV_REP, input->evbit);
    	input_set_capability(input, EV_MSC, MSC_SCAN);
    
    	input_set_drvdata(input, keypad_data);
    
    	irq_pin = of_get_named_gpio_flags(np, "gpio_int_pin", 0, (enum of_gpio_flags *)&config);
    	irq = gpio_to_irq(irq_pin);
    
    	//irq = client->irq;
    	//if (irq_is_gpio)
    	//	irq = gpio_to_irq(irq);
    
    	error = devm_request_threaded_irq(dev, irq, NULL, tca8418_irq_handler,
    					  IRQF_TRIGGER_FALLING |
    						IRQF_SHARED |
    						IRQF_ONESHOT,
    					  client->name, keypad_data);
    	if (error) {
    		dev_err(dev, "Unable to claim irq %d; error %d\n",
    			client->irq, error);
    		return error;
    	}
    	//#endif
    
    
    	error = input_register_device(input);
    	if (error) {
    		dev_err(dev, "Unable to register input device, error: %d\n",
    			error);
    		return error;
    	}
    
    	return 0;
    }
    
    static const struct i2c_device_id tca8418_id[] = {
    	{ TCA8418_NAME, 8418, },
    	{ }
    };
    MODULE_DEVICE_TABLE(i2c, tca8418_id);
    
    #ifdef CONFIG_OF
    static const struct of_device_id tca8418_dt_ids[] = {
    	{ .compatible = "ti,tca8418", },
    	{ }
    };
    MODULE_DEVICE_TABLE(of, tca8418_dt_ids);
    
    /*
     * The device tree based i2c loader looks for
     * "i2c:" + second_component_of(property("compatible"))
     * and therefore we need an alias to be found.
     */
    MODULE_ALIAS("i2c:tca8418");
    #endif
    
    static struct i2c_driver tca8418_keypad_driver = {
    	.driver = {
    		.name	= TCA8418_NAME,
    		.of_match_table = of_match_ptr(tca8418_dt_ids),
    	},
    	.probe		= tca8418_keypad_probe,
    	.id_table	= tca8418_id,
    };
    
    static int __init tca8418_keypad_init(void)
    {
    	printk ("---Feibob: TCA8418\n");
    	return i2c_add_driver(&tca8418_keypad_driver);
    }
    subsys_initcall(tca8418_keypad_init);
    
    static void __exit tca8418_keypad_exit(void)
    {
    	i2c_del_driver(&tca8418_keypad_driver);
    }
    module_exit(tca8418_keypad_exit);
    
    MODULE_AUTHOR("Kyle Manna <kyle.manna@fuel7.com>");
    MODULE_DESCRIPTION("Keypad driver for TCA8418");
    MODULE_LICENSE("GPL");
    

  • This is the driver source code.

    Please show how you have configured the device.

  • Hi Reed,

    If you want to ensure that internal pull-up registers are enabled, please read registers GPIO_PULL1, GPIO_PULL2, GPIO_PULL3 (0x2C, 0x3D, 0x2E). These values should read back 0x00, 0x00, 0x00, if internal pull-ups are currently enabled. 

    If a bit value of 1 is present in the register, this means that the internal pull-up for that bit number is disabled. 

    Again, this information is found on page 34. of the TCA8418 datasheet. 

    Regards,

    Tyler