Part Number: SN75DPHY440SS
Hi,
What is the maximum insertion loss that SN75DPHY440SS can support?
Best regards,
Randy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN75DPHY440SS
Hi,
What is the maximum insertion loss that SN75DPHY440SS can support?
Best regards,
Randy
Randy
Please reference to this table.

So max insertion loss DPHY440 can compensate at 1GHz (500MHz) is 4dB and at 1.5GHz (750MHz) is 5dB.
On the TX side, we have pre-emphasis that can provide 2.5dB compensation.

Thanks
David
Luke
The DPHY440 does not support 2.5Gbps, therefore we do not need to specify the insertion loss at 2.5Gbps.
Thanks
David