This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX3232: Asking for MAX3232 design review and suggestions

Part Number: MAX3232

Hi Team,

Customer would like to design MAX3232. There is failed case among two chip. (1/2 failed case)

Target to MP soon. Would you please help review  schematic and provide your comments to see any abnormal on design?

 

For ok IC case, pin 9 is 5V.

For failed IC, pin 9 is 1.3V.

 

ABA swap experiment is verified.

RD also double checked the IC pin 9 impedance itself (remove IC from PCB board). No obviously difference on pin9.

 

Here is the design material.

https://txn.box.com/s/eakysnmfo1octjuq5n7md37jwozt5dm4

 

 

 

Thanks for help!

 

SHH