Part Number: DP83630
Hi All,
I have a question about the DP83630.
If I don't use the LED_ACT pin, can I leave it open?
Or do you need to do pullups and pulldowns?
If the default option is required, then there is no need for external pull-up or pull down resistors.
The datasheet contained the following:
" If the default option is required, then there is no need for external pull-up or pull down resistors. "
Therefore, I think that there is no problem even if it is Open.
Best Regards,
Ishiwata