Part Number: SN65HVD232
Hi, Im using SN65HVD232 in my design suppled with 3.3V. but the CAN High voltage im is getting 3.6V whereas as per datasheet CANH voltage level is is 2.45 to VCC.


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD232
Hi, Im using SN65HVD232 in my design suppled with 3.3V. but the CAN High voltage im is getting 3.6V whereas as per datasheet CANH voltage level is is 2.45 to VCC.


It is not possible for this driver to drive higher than its own supply.
Is this packet really sent from this SN65HVD232? The ACK bit shows that there are multiple transceivers on the bus.
Is the ground the same at the transceiver and at the place where you are measuring?
Hi Vvn,
Because SN65HVD232 is supplied by a 3.3V rail, it is not possible for this device to generate a voltage of 3.6V. This CANH level is much more typical of a 5V supplied transceiver. Have you tried disconnecting the SN65HVD232 node from the rest of the CAN bus the take this measurement? You may also be able to find a different CAN frame that is driven by the 3.3V transceiver on the scope by capturing a few times until you see the correct voltage levels or by triggering off of the TXD signal of the SN65HVD232 if this is accessible. Make sure that this CAN node has data to transmit and is not just a passive listening node.
Regards,
Eric Schott