Part Number: TCAN1048AV-Q1
Hi,
I am using TCAN1048AVDMTRQ1 integrated. When I run STB1 and STB2 pins high (standby mode), I see data on the line, but when I operate STB1 and STB2 pins low (normal mode), I cannot see data on the line.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1048AV-Q1
Hi,
I am using TCAN1048AVDMTRQ1 integrated. When I run STB1 and STB2 pins high (standby mode), I see data on the line, but when I operate STB1 and STB2 pins low (normal mode), I cannot see data on the line.

Hi Onur,
The Standby input pins for TCAN1048A are inverse logic compared to TCAN1046A. This means for TCAN1048A, a high level input on pins 8 or 14 (nSTB2 and nSTB1) will put the device into normal mode, whereas a low level input on these pins will place the device into Standby mode.
If you would like a device that operates in the polarity that you describe, I recommend using the TCAN1046A.
Let me know if you have any more questions.
Regards,
Eric Schott