Other Parts Discussed in Thread: DS90UR241
We need to deserialize signal from ub303. Can ub928, ub924, ub940, ub948 be used in this case? If yes, need to set certain compatibility mode?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We need to deserialize signal from ub303. Can ub928, ub924, ub940, ub948 be used in this case? If yes, need to set certain compatibility mode?
Hello Wei,
Yes this is possible, but the allowable PCLK range must be constrained to fit the limits of both devices in the SER/DES pair. There is no special mode needed
Best Regards,
Casey
All of the four deserializers mentioned are compatible? We have no control over the ub303 PCLK. What should we do to constrain the PCLK of the deserializers? Thank you.
Wei,
Yes, all 4 are compatible. The PCLK comes from the source that is attached to the UB303. So as long as UB303 is operated within datasheet limits, then all 4 of these DES can be supported since the UB303 has a more narrow PCLK range than any of these DES.
Best Regards,
Casey
Hi Casey,
Are any of the four deserializers compatible with ds90ur241 in backward compatibility mode?
Thank you.
DS90UR905 and DS90UR907 are FPD-LINK II devices, but they are said to be compatible with UB924 and UB928 in their data sheets. DS90UR906 is also compatible with DS90UR241 according to the data sheet. However, DS90UR241‘s compatibility with FPD-LINK III devices are never mentioned in data sheets, although some say they are compatible.
Wei,
DS90UR241 is not compatible to FPD III devices. It is an older generation 18 bit color serializer from the FPD II generation. 906 is a newer FPD II generation which supports 24 bit color but also had a backwards compatible mode to UR241. But 92x and 94x don't have compatibility all the way back to UR241.
Best Regards,
Casey
Is there a device that is compatible with ur241, ur905 and ur925 all three? Thanks
Hello Wei,
No, there is no single device with this compatibility
Best Regards,
Casey