hi team,
as datasheet says VCCB should be higher than VCCA, but the figure 13 in the datasheet shows VCCA and VCCB are connected together.
so can we connected VCCA and VCCB in to the same power supply? thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi team,
as datasheet says VCCB should be higher than VCCA, but the figure 13 in the datasheet shows VCCA and VCCB are connected together.
so can we connected VCCA and VCCB in to the same power supply? thanks.
Hi Clemens,
Thx a lot for confirming that VCCA and VCCB being using the same power supply is allowed.
And please let me use this opportunity to make another question clearer. In the TCA9617A, it states that "VCCB should always be higher than VCCA. VCCB cannot be lower than VCCA even when the device is disabled."
But as your comments above, do you mean that VCCA being higher than VCCB by up to 0.5V is acceptable?
BR,
Jon
Cai,
Clemmen's response is correct. The TCA9617 (both A and B) allow for VCCA=VCCB as long as the recommended operating voltage is being followed.
Clemen's response about the 0.5V margin is related to why VccA should not be larger than VccB. In the A version, there is a leakage path from A side to B side, to get this leakage path to actually leak, you would need to have VccA larger than VccB by a threshold voltage, 0.5V is close to that value.
-Bobby