This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DPHY440SS: In a CSI application, is it possible to invert N and P on both sides of the chip except for the clk ?

Part Number: SN65DPHY440SS


Hi,

I want to use the SNx5DPHY440SS as a CSI retimer on an interface board in between two connectors

To facilitate the layout and have cleaner traces i would like to connect the DPHY in the following way :

To sum up :

connector 1  |  DPHY440  |  connector 2

¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬¬

D0N               |   DA/B0 P    |  D0N

D0P               |   DA/B0 N    |  D0P

D2N               |   DA/B1 P    |  D2N

D2P                |   DA/B1 N    |  D2P

CLK   P          |     CLK   P    |  CLK   P

CLK   N          |     CLK   N    |  CLK   N

D3N               |   DA/B2 P    |  D3N

D3P               |   DA/B2 N    |  D3P

D1P               |   DA/B3 P    |  D1P

D1N              |   DA/B3 N    |  D1N

From the datasheet and other questions on the forum, it seems that plugging any lane number anywhere on the DPHY440 is fine if the lane number are kept identical on the camera and CPU in a CSI application

The datasheet states that the DPHY440 doesn't support inverting polarity on the data lanes but if lanes are inverted on both sides of the DPHY, does it works ?
Do we need to invert all the lanes for this to work ? As in my schematic, the clock and the channel 3 are not inverted


Also, it seems from other posts in the forum that for the DPHY to work in the CSI 4 lane configuration, it needs some i2c commands to be send, is it so ?
( From other posts on that forum :

Write Register 0x50 with 8’h01 //Override enable for HS TX path

Write Register 0x51 with 8’h01 //HS TX path enabled.

Write Register 0x61 with 8’h00  // Disable LP path.

Write Register 0x70 with 8’h01  //Override enable for HS RX path

Write Register 0x71 with 8’h01  // HS RX path enabled.

Bit 0 is lane 0

)

Thanks a lot in advance,

Sylvain

  • Sylvain

    The DPHY440 can't support polarity inversion, the above proposal will not work in DPHY440 default state. The high speed entry sequence consists of driving LP11->LP01->LP00 (LP->HS transition). If you flip the polarity, then the high speed entry sequence will be flipped as well and you will never able to enter into HS mode. 

    The only way it will work is that if the DPHY440 is in I2C mode and only HS mode is always enabled using the following sequence. The sequence puts the CLK and all data lanes into HS mode only.

    Write Register 0x50 with 8’h1F //Override enable for HS TX path

    Write Register 0x51 with 8’h1F //HS TX path enabled.

    Write Register 0x61 with 8’h00  // Disable LP path.

    Write Register 0x70 with 8’h1F  //Override enable for HS RX path

    Write Register 0x71 with 8’h1F  // HS RX path enabled.

    Thanks

    David