Part Number: DS90UB941AS-Q1
Hi,
I am with an issue regarding the LINK_DETECT bit in register GENERAL_STS Register (Address = 0xC). I have 2 displays connected in the IC, one in the port 0 and another in the port 1. I need to detect when one cable from the monitors is disconnected. But the LINK_DETECT register( bit 0) is only detecting when the display in port 1 is disconnected, it is not detecting when the display in port 0 is disconnected.
Are there another register I need to look or configure to enable detect of loss in port 0?