Hi Expert,
my customer is using SN65HVD33DR SOIC-14, for Pin 5, Digital input, the input signal will have overshoot and undershoot, the max and min will be 4.05V and -1.10V. our absolute electric parameter in the datasheet is

here is the input signal, do we have any limitation for input overshoot and undershoot? if no, any risk in this scenario?

here is the input signal, overshoot max is 4.05V, undershoot is -1.10V. high level is 3.26V, low level is 50mV.
BR
Chi