Part Number: AM26LV31
Other Parts Discussed in Thread: AM26LV32
On my mother board, I am using the AM26LV31 to send step and direction bits to a remote servo controller. (over about 6 feet of wire)
This wire is terminated with a 4.7 ohms in series, and a 120 Ohm termination resistor with TVS diodes on both sides,
and the receiving chip is a AM26LV32 (This is on the servo controller)
The problem is now on at least 3 machines, the outputs of the AM26LV31 have blown out.
If I measure the output to ground, its 4 ohms. Some chips its 450K (I think this is a good chip),
other chips have measured 40K, even down to 4.5k
What could the explanation be as to why this chip blew out?
and what can I do to protect it?
Admittedly, I have no protection on the mother board side, the chip outputs go directly to a connector.
Thanks for any advice!