Part Number: DP83848J
Hi,
I need to communicate between a microcontroller that has an integrated MAC (datasheet : URL) and a microprocessor that has an integrated MAC and PHY (datasheet : URL). The pins of the MAC on the processor are already used by design, so I plan to use the DP838484JSQ/NOPB between the two. Here is the schematics :

The chips are on the same board. There will not be a RJ45 connector. The maximum distance between them will be some centimeters. I do not know yet if I will use 10 or 100 Mbps.
My questions are as follows:
- Do I need a transformer on the 10BASE-T/100BASE-TX lines? I think I do, based on the page 65/87 of the datasheet of the DP83848 : URL
- If so, would this one suits : URL ?
- Do I need a transformer on the RMII lines as well? BOM cost is a real concern for the project, so if it can work without a second transformer that would be great.
Thank you for your answer.