Hi,
Can I use one of the GPIOs to send a clock from the DS90UB953A-Q1? If yes, what the frequency it can drive?
shmuel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can I use one of the GPIOs to send a clock from the DS90UB953A-Q1? If yes, what the frequency it can drive?
shmuel
Ho Logan,
I want to use 1 GPIO of the 953 and connet it to a clock to a FPGA.
As I understand from your answer I can drive 25/12.5/5Mhz.
Is it depen the mode the 953 is working?
BR
Shmuel
Hi Shmuel,
This table example is specifically for 4-Gbps synchronous mode with REFCLK = 25 MHz. See more details in the Forward Channel GPIO section of the datasheet.
Regards,
Logan